Hello,
I wanted to know if it was possible to make an assertion of the Power on reset of the IMX8X apart from the PMIC PF8100 / PF8200 (via a parallel secondary circuit).
Moreover in case of Power on reset on the IMX8X, the output SCU_WDOG_OUTSCU_WDOG_OUT is not asserted?
Thank you.
Best Regards Vincent Massonneau.
已解决! 转到解答。
Hi vincent_massonn
>I wanted to know if it was possible to make an assertion of the Power on reset of the
>IMX8X apart from the PMIC PF8100 / PF8200 (via a parallel secondary circuit).
in general yes, one can use some gpio for controlling such external circut.
>Moreover in case of Power on reset on the IMX8X, the output
>SCU_WDOG_OUTSCU_WDOG_OUT is not asserted?
it depends on reset type, for case "partition" reset it is not asserted as described on below
https://community.nxp.com/t5/i-MX-Processors/Watchdog-AP-cores-on-imx8QM-MEK/m-p/1153684
Types of reset are described in sect.13.7 TIMER: Timer Service sc_fw_api_qx_b0.pdf
included in SCFW Porting Kit
Best regards
igor
Hi vincent_massonn
>I wanted to know if it was possible to make an assertion of the Power on reset of the
>IMX8X apart from the PMIC PF8100 / PF8200 (via a parallel secondary circuit).
in general yes, one can use some gpio for controlling such external circut.
>Moreover in case of Power on reset on the IMX8X, the output
>SCU_WDOG_OUTSCU_WDOG_OUT is not asserted?
it depends on reset type, for case "partition" reset it is not asserted as described on below
https://community.nxp.com/t5/i-MX-Processors/Watchdog-AP-cores-on-imx8QM-MEK/m-p/1153684
Types of reset are described in sect.13.7 TIMER: Timer Service sc_fw_api_qx_b0.pdf
included in SCFW Porting Kit
Best regards
igor