Dear friend
My platform is i.MX8QXP, SJA1105, Yocto L5.4.70_2.3.0.
description:
1)SJA1105's port0 connect to i.MX8QXP's ethphy0,
2)SJA1105's SPI connect to i.MX8QXP's LSPI2;
Question:
1)can you provide an device tree example for SJA1105 connected to i.MX8QXP according to my description?
----
BR
解決済! 解決策の投稿を見る。
all of SJA1105Q materials you can find from the link as below, you can refer to the dts file as below:
"https://source.codeaurora.org/external/autoivnsw/sja1105x_linux_switchdev/tree/doc/device_tree"
all of SJA1105Q materials you can find from the link as below, you can refer to the dts file as below:
"https://source.codeaurora.org/external/autoivnsw/sja1105x_linux_switchdev/tree/doc/device_tree"