Dear NXP Team,
We are exploring options to connect an SATA SSD to our custom-designed IMX8QXP board, but we've observed that the processor lacks SATA support. Therefore, we are considering connecting an NVMe-based SSD via the PCIe interface on the M.2 connector instead. Could you confirm if this is feasible? Also, do we have driver support available for this configuration?
checked the imx8qxp schematic, which support M.2 KEY E, if you need connect SSD via M.2 connector, you need convert M.2 KEY E to M.2 KEY M to support this, the cable like this
Sintech M.2 (NGFF) NVME SSD to M2 A/E Key WiFi Port with 20cm Cable