Hello community,
Some community thread were talk about iMX8QM ISI errata
ERR050066: ISI: Data overflows occur when input streams exceed AXI transaction frequency
like this.
8 x 1080p MIPI CSI2 cameras capture in iMX8QM
In this errata
"However, combinations of sensors which add
up to less than 2Mpixel are supported with current design."
mean that
1) 2Mpixel mean that 1920x1080 = 2,073,600 is correct?
2) How about frame rate.1920x1080 @60 or 1920x1080 @30
Does this apply to each channel individually?
Can it capture for 2ch 1920x1080 @60 support?
MIPI-CSI2_0 | 1920 x 1080 @60 |
MIPI-CSI2_1 | 1920 x 1080 @60 |
The other hand, i.MX8QXP_C0 silicon have no errata "ERR050066: ISI: Data overflows occur when input streams exceed AXI transaction frequency"..
Is it support 4K@30 video capture?
device | ch | resolution | fps |
i.MX8QM | 2 | 1920x1080 | 60 |
i.MX8QP | 2 | 1920x1080 | 60 |
i.MX8QXP | 1 | 3840x2160 | 30 |
Best regards,
Ishii
已解决! 转到解答。
the mipi csi capture max is 6Gbps, so should can support 4k, but we didn't test this, maybe would have issue when capture 4k, only test resolution is 1280x800@30, we didn't test 6Gbps, I think 6Gbps maybe cause some bandwidth issue, I only can say we tested max thoughout is 4x1280x800@30
I would like to follow up on the iMX8QM CSI2 Bandwidth.
In the TRM I have the following information about the clocks used in CSI-2 module.
With a single pixel interface, data_out contains a single pixel every clock that dav_out
(data valid) is asserted. The single pixel interface must run at a frequency that is equal to
number of MIPI lanes times the byte lane frequency.clk :
RX Controller Core Clock input. This clock must be exactly equal to or faster than the receive byteclock, RxByteClkHS_ln0, from the RX DPHY.clk: SSSLICE2 : LPCG_MIPI_CSI_LPCG_24
clk_ui:
User interface clock. The frequency of clk_ui must be such that the data received on the data_out output is greater than or equal to the total bandwidth of the physical MIPI interface. Clk_ui has no relationship requirement with regards to ‘clk’ other than the bandwidth requirement mentioned previously.clk_ui: SSSLICE2: LPCG_MIPI_CSI_LPCG_24
From the clock subsystem, CLK and CLK_UI have the same frequency.
Can the CSI-2 block process all the data when all 4 lanes are receiving at 1.5Gbps ?
clk is generated from DIG_PLL0 @ 720 MHZ, a divider provides 360MHz. Can clk be provided a higher frequency ?
Based on the TRM : clk >= lanes * mipi_lane_freq*DDR / 8 >= 4*2/8 * mipi_lane_freq.
Am I correct to add all the lanes byteclock for the overall receive byteclock ?
Is there a bandwidth limitation at the CSI-2 level ?
CSI-2 6Gbps would need 16.666 x 360MHz. I am not sure of the internal bus width that processes the Rx DPHY data.
Hello @joanxie
Thank you for your reply.
How about color format of tested capture 4x1280*800@30Hz.
It is boundary of ISI limitation.
4x1280*800@30Hz*3Byte(RGB24bit) > 2Mpixel(ISI limit) > 4x1280*800@30Hz*2Byte(YUYV16bit)
Best regards,
Ishii.
Hello @joanxie
Thank you for your reply.
You say that "only tested 4x1280*800@30Hz successfully, so for 4k@30,"
I understand that only tested 4x1280*800@30Hz successfully,
throughput of this condition is lager than 2Gbps, so iMX8QM capture can support more than 2Gbps.
That is, the ISI limit is not affected, so the maximum supported size is 4K@30.
But if test condition is 4x1280*800@30Hz x 16bit/pixel,
This explanation is not valid. Because throughput of test condition is less than 2Gbps.
Which is correct?
1) Maximum capture size of iMX8QM is unknown.
2) It has no test but it supports 6Gbps, so it will be 4K@30.
Sorry to keep checking back, but we need accurate information on this specification
as it is an important issue that affects product planning.
Best regards,
Ishii.
the mipi csi capture max is 6Gbps, so should can support 4k, but we didn't test this, maybe would have issue when capture 4k, only test resolution is 1280x800@30, we didn't test 6Gbps, I think 6Gbps maybe cause some bandwidth issue, I only can say we tested max thoughout is 4x1280x800@30
Hello @ShrithiR ,
> Here what is 4? Is it data lanes?
No, 4 is a camera input count in this formula.
Please see NXP surround view system web.
Best regards,
Ishii.
Hello @joanxie
Thank you for your reply.
I understand that ISI errata050066 does not affect the capture performance of MIPI-CSI2, so MIPI-CSI2 capture max is 6Gbps and it should can support 4k.
Best regards,
Ishii.
Hello @joanxie
Please teach me a byte/pixel size of capture test for 4x 1280*800@30Hz
If it is 2byte/pixel = YUYV, the data volume for this test is less than 2 Gbps.
4x 1280`800 * 30 * 2byte/pixel = 1.966Gbps
This result does not prove that 4K capture is possible because it falls within the errata constraints.
I would appreciate your immediate attention to this matter.
Best regards,
Ishii.
Hello @joanxie
Thank you for your reply.
In Figure 15-1. Interconnection Diagram of Reference Manual IMX8QMRM Rev. 0,
MIPI-CSI2 connect to ISI.
So, MIPI-CSI2 can supports 6Gbps so it can capture 4K@30,
Bat ISI have performance limitation 2MPixel.
I think that it is ok to use i.MX8QXP_C0 silicon because it is fixed this limitation.
But i.MX8QM have no C0 revision.
Is it can really capture 4K@30? to frame memory on DDR?
Best regards,.
Ishii.