Hello,
We are using a custom design board based off the 8MNANOD4-EVK. Same DRAM and PMIC
The tool successfully downloads to board but never continue after that point.
Download is complete
Waiting for the target board boot...
===================hardware_init=====================
********Found PMIC BD718XX**********
hardware_init exit
*************************************************************************
*************************************************************************
*************************************************************************
MX8 DDR Stress Test V3.20
Built on Feb 23 2021 13:49:21
*************************************************************************
Waiting for board configuration from PC-end...
Why would It be stuck at this step?
解決済! 解決策の投稿を見る。
Turns out the UART RX on the processor was not hooked up correctly.