IMX8Nano DDR Tool Stuck On Waiting for board configuration from PC-end...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8Nano DDR Tool Stuck On Waiting for board configuration from PC-end...

Jump to solution
1,093 Views
scvi
Contributor II

Hello,

We are using a custom design board based off the 8MNANOD4-EVK. Same DRAM and PMIC

The tool successfully downloads to board but never continue after that point.

 

 

Download is complete
Waiting for the target board boot...

===================hardware_init=====================

********Found PMIC BD718XX**********
hardware_init exit

*************************************************************************

*************************************************************************

*************************************************************************
       MX8 DDR Stress Test V3.20
       Built on Feb 23 2021 13:49:21
*************************************************************************

Waiting for board configuration from PC-end...

 

 

Why would It be stuck at this step?

0 Kudos
Reply
1 Solution
1,087 Views
scvi
Contributor II

Turns out the UART RX on the processor was not hooked up correctly.

View solution in original post

0 Kudos
Reply
1 Reply
1,088 Views
scvi
Contributor II

Turns out the UART RX on the processor was not hooked up correctly.

0 Kudos
Reply