Hi,
I've been trying to bring up the board using the "Serial Download Mode" and the UUU tool found here https://github.com/nxp-imx/mfgtools. UUU got built fine in WSL. The board gets brought up fine in eMMC boot and SD boot mode with "Linux 6.1.1_1.0.0" image. However, for USB boot to work we need a USB connection to PC. This connection is not being recognised by PC.
When running ./uuu -lsusb I get the following:
There are 4 USB connectors on the EVK.
1) J23, Micro USB Serial UART connection
2) J5, USB-C Power connection
3) J6, USB-C Port 1 DRP connection
4) J7, USB-A Port 2 Host connection
I've connected Port 1 to my PC which doesn't seem to get recognised.
The board: https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-...
已解决! 转到解答。
Issue is caused due to having UUU installed on WSL which is not able to read USB ports natively.