IMX8MPLUSLPD4-PEVK USB Boot not detected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MPLUSLPD4-PEVK USB Boot not detected

ソリューションへジャンプ
1,938件の閲覧回数
MartinKozevnikov
Contributor II

Hi,
I've been trying to bring up the board using the "Serial Download Mode" and the UUU tool found here https://github.com/nxp-imx/mfgtools. UUU got built fine in WSL. The board gets brought up fine in eMMC boot and SD boot mode with "Linux 6.1.1_1.0.0" image. However, for USB boot to work we need a USB connection to PC. This connection is not being recognised by PC. 

When running ./uuu -lsusb I get the following:

MartinKozevnikov_0-1681305077158.png

There are 4 USB connectors on the EVK. 
1) J23, Micro USB Serial UART connection
2) J5, USB-C Power connection
3) J6, USB-C Port 1 DRP connection
4) J7, USB-A Port 2 Host connection

I've connected Port 1 to my PC which doesn't seem to get recognised.

The board: https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-... 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,919件の閲覧回数
MartinKozevnikov
Contributor II

Issue is caused due to having UUU installed on WSL which is not able to read USB ports natively. 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,920件の閲覧回数
MartinKozevnikov
Contributor II

Issue is caused due to having UUU installed on WSL which is not able to read USB ports natively. 

0 件の賞賛
返信