IMX8M-EVK M.2 PCIE port

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8M-EVK M.2 PCIE port

跳至解决方案
818 次查看
rahmanuh
Contributor III

Hello,

I found out a while ago that if I want to use PCIE-USB WiFi module for MCIMX8M-EVKB, I need to rework the EVK board by pupolate/depopulate some resistors. As I find it is very difficult for me to do so, I think I should use another interface (i.e PCIE-UART WiFi module). I see in the MCIMX8M-EVKB schematic, it seems I can use PCIE-UART out of the box without modification. Could anyone kindly confirm this?

Thank you very much.

Kind regards,
Rahmanu

标签 (1)
0 项奖励
回复
1 解答
809 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rahmanu

 

yes it can be used, both PCIe and UART signals are connected to M.2 (J1401)

on SPF-38820 i.MX8MQ EVK schematic   Design Files for the i.MX 8M Evaluation Kit (EVKB)

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
1 回复
810 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rahmanu

 

yes it can be used, both PCIe and UART signals are connected to M.2 (J1401)

on SPF-38820 i.MX8MQ EVK schematic   Design Files for the i.MX 8M Evaluation Kit (EVKB)

 

Best regards
igor

0 项奖励
回复