IMX8M-EVK M.2 PCIE port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M-EVK M.2 PCIE port

ソリューションへジャンプ
840件の閲覧回数
rahmanuh
Contributor III

Hello,

I found out a while ago that if I want to use PCIE-USB WiFi module for MCIMX8M-EVKB, I need to rework the EVK board by pupolate/depopulate some resistors. As I find it is very difficult for me to do so, I think I should use another interface (i.e PCIE-UART WiFi module). I see in the MCIMX8M-EVKB schematic, it seems I can use PCIE-UART out of the box without modification. Could anyone kindly confirm this?

Thank you very much.

Kind regards,
Rahmanu

ラベル(1)
0 件の賞賛
返信
1 解決策
831件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rahmanu

 

yes it can be used, both PCIe and UART signals are connected to M.2 (J1401)

on SPF-38820 i.MX8MQ EVK schematic   Design Files for the i.MX 8M Evaluation Kit (EVKB)

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
832件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rahmanu

 

yes it can be used, both PCIe and UART signals are connected to M.2 (J1401)

on SPF-38820 i.MX8MQ EVK schematic   Design Files for the i.MX 8M Evaluation Kit (EVKB)

 

Best regards
igor

0 件の賞賛
返信