Solved! Go to Solution.
It is OCOTP_CFG6(OTP Bank 0, word 7) bit 3.
You can use fuse command in uboot to disable the SD/MMC manufacture mode.
But I suggest you could keep this usesful function for recovery or mass production.
Are you using the NXP reference board?
It is a simple reason.
The usdhc1 is SD/MMC manufacture mode interface.
Before i.MX6ULL goes to serial download mode, it will check the SD/MMC manufacture mode interface first.
It is a clear scenario in i.MX6ULL reference manual.
Hello rudi ,
Thank you for your quick response ,
So can you suggest any solution for how can we disable it using efuse bits.?
if you have any documentation OR example then please let us know.
Thanks and Regards
It is OCOTP_CFG6(OTP Bank 0, word 7) bit 3.
You can use fuse command in uboot to disable the SD/MMC manufacture mode.
But I suggest you could keep this usesful function for recovery or mass production.