Now we need add tw6865 ic to imx6q board,
but when start kernel tw6865 prob could be failed,
and the log file indicated that can't enable device BAR0 not claimed,
i have uploaded the log picture as attachment, please help check this issue , thanks a lot
This could be due to hardware connection issues between IMX6Q and the chip. Which kernel and distribution you use? Couple of things you can try in the kernel to tweak :
1. Try disabling PCI Force Gen 1 option in menuconfig
2. Also disable PCIE MSI Signal Interrupt Option
Regards
Anuradha