IMX6q 上添加tw6865芯片时注册失败

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6q 上添加tw6865芯片时注册失败

1,641 Views
joubertshe
Contributor I

Now we need add tw6865 ic to imx6q board,

but when start kernel tw6865 prob could be failed,

and the log file indicated that can't enable device BAR0 not claimed,

i have uploaded the log picture as attachment, please help check this issue , thanks a lot

Tags (2)
0 Kudos
Reply
3 Replies

1,129 Views
tengri
Contributor IV

This could be due to hardware connection issues between IMX6Q and the chip. Which kernel and distribution you use? Couple of things you can try in the kernel to tweak :

1. Try disabling PCI Force Gen 1 option in menuconfig

2. Also disable PCIE MSI Signal Interrupt Option

Regards

Anuradha

0 Kudos
Reply

1,129 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the topic here:

https://community.nxp.com/thread/444870 

0 Kudos
Reply

1,129 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the link as below, you can refer to the software path.

https://community.nxp.com/docs/DOC-94541 

0 Kudos
Reply