IMX6SX PCIE 驱动问题

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6SX PCIE 驱动问题

1,605件の閲覧回数
jingyangxie
Contributor V

最近在使用imx6sx sdb板,BSP版本为4.1.15,按照《i.MX_Linux_Reference_Manual》的要求,做如下配置:

1.png

系统运行后,执行lspci,没有任何内容出现,请问在IMX6SX中如何配置和加载PCIE驱动

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,324件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

which PCIe device are you connected to?

0 件の賞賛
返信

1,324件の閲覧回数
jingyangxie
Contributor V

我是fpga模拟出的pcie设备,使用3.14.52版本的内核可以,但是3.14.52和4.1.15的架构差的比较多,不知道从何分析

发自网易邮箱大师

在2016年10月27日 16:45,jimmychan 写道:

|

|

NXP Community

|

|

Re: IMX6SX PCIE 驱动问题

reply from jimmychan in i.MX Community - View the full discussion

which PCIe device are you connected to?

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in i.MX Community by email or at NXP Community

Following Re: IMX6SX PCIE 驱动问题 in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

|

|

0 件の賞賛
返信