IMX6S spread spectrum for PLL2 PFD[0:2]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6S spread spectrum for PLL2 PFD[0:2]

ソリューションへジャンプ
1,332件の閲覧回数
kanoumamoru
Contributor III

Hi,

As my understanding PLL2 (system PLL) 528Mhz only supports the spread spectrum in i.MX6S.

Does the PLL2_PFDs (PFD0=352MHz, PFD1=594MHz, PFD2=396MHz) also should support the spread spectrum ?

PLL2_PFD is deriverd form PLL2 according to following formula.

PLL2_PFD =  PLL2 * (18/N)

(N is from 12 to 35)

According to additional PLL2_PFD, the function of the spread spectrum fades away ?

Regards,

Kanou

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
741件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mamoru

>As my understanding PLL2 (system PLL) 528Mhz only supports the spread spectrum in i.MX6S.

Correct.

>Does the PLL2_PFDs (PFD0=352MHz, PFD1=594MHz, PFD2=396MHz) also should support the spread spectrum ?

Yes, since they are sourced from PLL2. Description can be found in

EB790 Configuration of Phase Fractional Dividers

>According to additional PLL2_PFD, the function of the spread spectrum fades away ?

Yes if you are speaking about absolute value.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
742件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mamoru

>As my understanding PLL2 (system PLL) 528Mhz only supports the spread spectrum in i.MX6S.

Correct.

>Does the PLL2_PFDs (PFD0=352MHz, PFD1=594MHz, PFD2=396MHz) also should support the spread spectrum ?

Yes, since they are sourced from PLL2. Description can be found in

EB790 Configuration of Phase Fractional Dividers

>According to additional PLL2_PFD, the function of the spread spectrum fades away ?

Yes if you are speaking about absolute value.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信