IMX6Q and UBNT SR71

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q and UBNT SR71

955 Views
flohg
Contributor II

     Hello everyone!

I am currently trying to get a UBNT SR71 PCI-Express Card (Atheros AR928X) to work with my Imx6QRex-Board.

After some kernel setup the board is able to detect the card. My problem now is that I am not able to connect to another network or do a simple scan.

When I run "iwconfig wlan0 scan" I get the message "wlan0 No scan results". I tried different antennas and also exchanged the SR71 Module so I think it is not hardware related.

Is there some part of kernel configuration I am missing?

I am running the 3.0.35 kernel version, provided by Rex.

Best Regards,

Florian

Labels (2)
0 Kudos
Reply
3 Replies

815 Views
flohg
Contributor II

Thank you for the links - unfortunately, they did not help me very much. I tried to follow the guide for Android roughly (we do not and can not use Android - so I have some kind of ubuntu running.

Put even with the Kernel settings, I am still only able to see the device, but not able to connect to a network or scan for networks.

Best Regards,

Florian

0 Kudos
Reply

815 Views
igorpadykov
NXP Employee
NXP Employee

Hi flohg

I would suggest first verify it with linux.

Also it may be recommended to apply to Silex for

updated firmware for this module.

Best regards

igor

0 Kudos
Reply

815 Views
igorpadykov
NXP Employee
NXP Employee

Hi flohg

similar Atheros AR928X is also used in Silex SX-PCEAN(P)  (Atheros AR9280),

Silex modules are well supported for i.MX6, please check below links

How to Enable PCIe WiFi into i.MX6 Android Release?

Wireless Expertise | Wi-Fi for Freescale i.MX6 Processors | Silex Technology

How to add Wi-Fi to Freescale i.MX 6 - YouTube

Best regards

igor

0 Kudos
Reply