IMX6Q-SDB board is not booting with pre-built Image.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6Q-SDB board is not booting with pre-built Image.

3,331 次查看
ThanarajS
Contributor III

Hi,

I have IMX6Q SABRE SDB bouard.

I am using pre-build android image to get display on HDMI interface. (android_KK4.4.3_2.0.0-ga_core_source ).

When I start booting,  I got the below debug prints

U-Boot 2014.04-08637-gaffa032 (Apr 18 2016 - 14:09:54)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

CPU:   Temperature 24 C, calibration data: 0x5ab4f27d

Reset cause: POR

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

Found PFUZE100 deviceid=10,revid=11

check_and_clean: reg 0, flag_set 0

Fastboot: Normal

flash target is MMC:1

Net:   FEC [PRIME]

Normal Boot

Hit any key to stop autoboot:  0

booti mmc1

kernel   @ 14008000 (6723112)

ramdisk  @ 15000000 (497370)

fdt      @ 14f00000 (50782)

kernel cmdline:

        use boot.img command line:

        console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=400M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.serialno=152041d4df669009

switch to ldo_bypass mode!

   Using Device Tree in place at 14f00000, end 14f0f65d

Starting kernel ...

Booting Linux on physical CPU 0x0

Initializing cgroup subsys cpu

Initializing cgroup subsys cpuacct

Linux version 3.10.53-88098-g1c3a910 (root@test) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #1 SMP PREEMPT Mon Apr 18 09:57:34 IST 2016

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 Quad SABRE Smart Device Board

cma: CMA: reserved 384 MiB at 32000000

Memory policy: ECC disabled, Data cache writealloc

PERCPU: Embedded 8 pages/cpu @817d9000 s9728 r8192 d14848 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 259840

Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=400M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.serialno=152041d4df669009

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 959MB 64MB = 1023MB total

Memory: 627668k/627668k available, 420908k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0xc0800000 - 0xff000000   (1000 MB)

    lowmem  : 0x80000000 - 0xc0000000   (1024 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .text : 0x80008000 - 0x80e51868   (14631 kB)

      .init : 0x80e52000 - 0x80ea7600   ( 342 kB)

      .data : 0x80ea8000 - 0x80f2b740   ( 526 kB)

       .bss : 0x80f2b740 - 0x80fc02f8   ( 595 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Preemptible hierarchical RCU implementation.

NR_IRQS:16 nr_irqs:16 16

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

CPU identified as i.MX6Q, silicon rev 1.2

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Security Framework initialized

SELinux:  Initializing.

Mount-cache hash table entries: 512

Initializing cgroup subsys debug

Initializing cgroup subsys freezer

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x807bf708 - 0x807bf760

CPU1: Booted secondary processor

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

CPU2: Booted secondary processor

CPU2: thread -1, cpu 2, socket 0, mpidr 80000002

CPU3: Booted secondary processor

CPU3: thread -1, cpu 3, socket 0, mpidr 80000003

Brought up 4 CPUs

SMP: Total of 4 processors activated (6324.22 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

pinctrl core: initialized pinctrl subsystem

regulator-dummy: no parameters

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

Use WDOG2 as reset source

syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered

vdd1p1: 800 <--> 1375 mV at 1125 mV

vdd3p0: 2800 <--> 3150 mV at 3000 mV

vdd2p5: 2000 <--> 2750 mV at 2425 mV

cpu: 725 <--> 1450 mV

vddpu: 725 <--> 1450 mV

vddsoc: 725 <--> 1450 mV

syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered

syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered

!!request miniPCIE Power On gpio

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

bio: create slab <bio-0> at 0

mxs-dma 110000.dma-apbh: initialized

usb_otg_vbus: 5000 mV

usb_h1_vbus: 5000 mV

wm8962-supply: no parameters

mipi_dsi_pwr_on: no parameters

sensor-supply: 3300 mV

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c i2c-0: IMX I2C adapter registered

i2c i2c-1: IMX I2C adapter registered

i2c i2c-2: IMX I2C adapter registered

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed

mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Initialized.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

pureg-dummy: no parameters

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 4, 65536 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

TCP: reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

Freeing initrd memory: 484K (85000000 - 85079000)

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

imx6_busfreq busfreq.16: DDR medium rate not supported.

Bus freq driver module loaded

bt power gpio is:2

mxc_bt_rfkill driver success loaded

rfkill: BT RF going to : on

mxc_bt_rfkill_reset

mxc_ir consumer_ir.41: unable to request PWM.

platform consumer_ir.41: Driver mxc_ir requests probe deferral

console [pstore-1] enabled

ramoops: attached 0x100000@0x4bf00000, ecc: 0/0

mxc_ramoops device success loaded

futex hash table entries: 1024 (order: 4, 65536 bytes)

audit: initializing netlink socket (disabled)

type=2000 audit(0.480:1): initialized

VFS: Disk quotas dquot_6.5.2

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

NTFS driver 2.1.30 [Flags: R/W DEBUG].

jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

fuse init (API version 7.22)

msgmni has been set to 1994

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

imx-weim 21b8000.weim: WEIM driver registered.

mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed

MIPI DSI driver module loaded

imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_DISP0_DAT9 already requested by 2084000.pwm; cannot claim for lcd.34

imx6q-pinctrl 20e0000.iomuxc: pin-101 (lcd.34) status -22

imx6q-pinctrl 20e0000.iomuxc: could not request pin 101 on device 20e0000.iomuxc

mxc_lcdif lcd.34: Error applying setting, reverse things back

imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_DISP0_DAT9 already requested by 2084000.pwm; cannot claim for lcd.34

imx6q-pinctrl 20e0000.iomuxc: pin-101 (lcd.34) status -22

imx6q-pinctrl 20e0000.iomuxc: could not request pin 101 on device 20e0000.iomuxc

mxc_lcdif lcd.34: Error applying setting, reverse things back

mxc_lcdif lcd.34: can't get/select pinctrl

mxc_lcdif: probe of lcd.34 failed with error -22

mxc_sdc_fb fb.30: registered mxc display driver ldb

imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

Console: switching to colour frame buffer device 128x48

mxc_sdc_fb fb.31: Can't get fb option for mxcfb1!

mxc_sdc_fb fb.32: Can't get fb option for mxcfb2!

mxc_sdc_fb fb.33: Can't get fb option for mxcfb3!

imx-sdma 20ec000.sdma: no iram assigned, using external mem

imx-sdma 20ec000.sdma: loaded firmware 1.1

imx-sdma 20ec000.sdma: initialized

pfuze100-regulator 1-0008: Full lay: 1, Metal lay: 1

pfuze100-regulator 1-0008: FAB: 0, FIN: 0

pfuze100-regulator 1-0008: pfuze100 found.

SW1AB: 300 <--> 1875 mV at 1150 mV

SW1C: 300 <--> 1875 mV at 1175 mV

SW2: 800 <--> 3300 mV at 3300 mV

SW3A: 400 <--> 1975 mV at 1500 mV

SW3B: 400 <--> 1975 mV at 1500 mV

SW4: 800 <--> 3300 mV at 3150 mV

SWBST: 5000 <--> 5150 mV at 5000 mV

VSNVS: 1000 <--> 3000 mV at 3000 mV

VREFDDR: 750 mV

VGEN1: 800 <--> 1550 mV at 1500 mV

VGEN2: 800 <--> 1550 mV at 1500 mV

VGEN3: 1800 <--> 3300 mV at 2800 mV

VGEN4: 1800 <--> 3300 mV at 1800 mV

VGEN5: 1800 <--> 3300 mV at 3000 mV

VGEN6: 1800 <--> 3300 mV at 3300 mV

Serial: IMX driver

2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

console [ttymxc0] enabled

21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX

21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 62) is a IMX

serial: Freescale lpuart driver

imx sema4 driver is registered.

[drm] Initialized drm 1.1.0 20060810

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop: module loaded

imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_KEY_COL1 already requested by 21f4000.serial; cannot claim for 2008000.ecspi

imx6q-pinctrl 20e0000.iomuxc: pin-128 (2008000.ecspi) status -22

imx6q-pinctrl 20e0000.iomuxc: could not request pin 128 on device 20e0000.iomuxc

spi_imx 2008000.ecspi: Error applying setting, reverse things back

m25p80 spi32766.0: found mr25h256, expected m25p32

m25p80 spi32766.0: mr25h256 (32 Kbytes)

spi_imx 2008000.ecspi: probed

tun: Universal TUN/TAP device driver, 1.6

tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>

CAN device driver interface

libphy: fec_enet_mii_bus: probed

fec 2188000.ethernet eth0: registered PHC device 0

PPP generic driver version 2.4.2

PPP BSD Compression module registered

PPP Deflate Compression module registered

PPP MPPE Compression module registered

NET: Registered protocol family 24

usbcore: registered new interface driver asix

usbcore: registered new interface driver ax88179_178a

usbcore: registered new interface driver cdc_ether

usbcore: registered new interface driver net1080

usbcore: registered new interface driver cdc_subset

usbcore: registered new interface driver zaurus

usbcore: registered new interface driver cdc_ncm

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

usbcore: registered new interface driver cdc_acm

cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters

usbcore: registered new interface driver usb-storage

usbcore: registered new interface driver usbserial

usbcore: registered new interface driver option

usbserial: USB Serial support registered for GSM modem (1-port)

ci_hdrc ci_hdrc.1: doesn't support gadget

ci_hdrc ci_hdrc.1: EHCI Host Controller

ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb1: Product: EHCI Host Controller

usb usb1: Manufacturer: Linux 3.10.53-88098-g1c3a910 ehci_hcd

usb usb1: SerialNumber: ci_hdrc.1

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

mousedev: PS/2 mouse device common for all mice

usbcore: registered new interface driver xpad

usbcore: registered new interface driver usb_acecad

usbcore: registered new interface driver aiptek

usbcore: registered new interface driver gtco

usbcore: registered new interface driver hanwang

usbcore: registered new interface driver kbtab

usbcore: registered new interface driver wacom

elan-touch 2-0010: elan - Read Hello Packet Failed

elan-touch: probe of 2-0010 failed with error -22

egalax_ts 1-0004: Failed to read firmware version

egalax_ts: probe of 1-0004 failed with error -5

egalax_ts 2-0004: Failed to read firmware version

egalax_ts: probe of 2-0004 failed with error -5

input: max11801_ts as /devices/soc0/soc.1/2100000.aips-bus/21a4000.i2c/i2c-1/1-0048/input/input0

i2c-core: driver [isl29023] using legacy suspend method

i2c-core: driver [isl29023] using legacy resume method

snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0

i2c /dev entries driver

ov5640_read_reg:write reg error:reg=300a

camera ov5640 is not found

ov5642_read_reg:write reg error:reg=300a

camera ov5642 is not found

ov5640_read_reg:write reg error:reg=300a

camera ov5640_mipi is not found

mxc_v4l2_output v4l2_out.38: V4L2 device registered as video16

mxc_v4l2_output v4l2_out.38: V4L2 device registered as video17

usbcore: registered new interface driver uvcvideo

USB Video Class driver (1.1.1)

gspca_main: v2.14.0 registered

mag3110 2-000e: check mag3110 chip ID

input: FreescaleMagnetometer as /devices/virtual/input/input1

input: eCompass as /devices/virtual/input/input2

mag3110 2-000e: mag3110 is probed

input: FreescaleAccelerometer as /devices/virtual/input/input3

mma8x5x device driver probe successfully

imx2-wdt 20c0000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)

device-mapper: uevent: version 1.0.3

device-mapper: ioctl: 4.24.0-ioctl (2013-01-15) initialised: dm-devel@redhat.com

Bluetooth: Virtual HCI driver ver 1.3

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCIATH3K protocol initialized

usbcore: registered new interface driver btusb

cpuidle: using governor ladder

cpuidle: using governor menu

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

mmc1: no vqmmc regulator found

mmc1: no vmmc regulator found

mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA

mmc2: no vqmmc regulator found

mmc2: no vmmc regulator found

mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA

mmc3: no vqmmc regulator found

mmc3: no vmmc regulator found

mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA

mmc2: new high speed SDHC card at address e624

Galcore version 5.0.11.25762

mmcblk2: mmc2:e624 SS08G 7.40 GiB

mmcblk2: p1 p2 p3 < p5 p6 p7 p8 > p4

mmcblk2: p4 size 13352010 extends beyond EOD, truncated

mmc3: new high speed DDR MMC card at address 0001

mmcblk3: mmc3:0001 SEM08G 7.39 GiB

mmcblk3boot0: mmc3:0001 SEM08G partition 1 1.00 MiB

mmcblk3boot1: mmc3:0001 SEM08G partition 2 1.00 MiB

mmcblk3rpmb: mmc3:0001 SEM08G partition 3 128 KiB

mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

mxc_asrc 2034000.asrc: mxc_asrc registered

mxc_vpu 2040000.vpu: VPU initialized

hidraw: raw HID events driver (C) Jiri Kosina

mmcblk3: p1 p2 p3 < p5 p6 p7 p8 p9 > p4

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

ashmem: initialized

logger: created 256K log 'log_main'

logger: created 256K log 'log_events'

logger: created 256K log 'log_radio'

logger: created 256K log 'log_system'

usbcore: registered new interface driver snd-usb-audio

mmcblk3: p4 size 13303808 extends beyond EOD, truncated

mmcblk3boot1: unknown partition table

mmcblk3boot0: unknown partition table

wm8962 0-001a: customer id 0 revision D

fsl-hdmi-dai hdmi_audio.17: failed to probe. Load HDMI-video first.

fsl-hdmi-dai: probe of hdmi_audio.17 failed with error -12

input: WM8962 Beep Generator as /devices/soc0/soc.1/2100000.aips-bus/21a0000.i2c/i2c-0/0-001a/input/input4

imx-wm8962 sound.28:  wm8962 <-> 202c000.ssi mapping ok

imx-audio-hdmi sound-hdmi.29: initialize HDMI-audio failed. load HDMI-video first!

NET: Registered protocol family 26

u32 classifier

    Actions configured

Netfilter messages via NETLINK v0.30.

nf_conntrack version 0.5.0 (15958 buckets, 63832 max)

ctnetlink v0.93: registering with nfnetlink.

NF_TPROXY: Transparent proxy support initialized, version 4.1.0

NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.

xt_time: kernel timezone is -0000

ip_tables: (C) 2000-2006 Netfilter Core Team

arp_tables: (C) 2002 David S. Miller

TCP: cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 10

mip6: Mobile IPv6

ip6_tables: (C) 2000-2006 Netfilter Core Team

NET: Registered protocol family 17

NET: Registered protocol family 15

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

can: raw protocol (rev 20120528)

can: broadcast manager protocol (rev 20120528 t)

can: netlink gateway (rev 20130117) max_hops=1

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: BNEP socket layer initialized

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

Bluetooth: HIDP socket layer initialized

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

VGEN1: disabling

SWBST: disabling

SW4: disabling

wm8962-supply: disabling

usb_otg_vbus: disabling

regulator-dummy: disabling

imx mcc test is registered.

file system registered

android_usb gadget: Mass Storage Function, version: 2009/09/11

android_usb gadget: Number of LUNs=1

lun0: LUN: removable file: (no medium)

android_usb gadget: android_usb ready

input: gpio-keys.27 as /devices/soc0/gpio-keys.27/input/input5

snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)

ALSA device list:

  #0: wm8962-audio

Freeing unused kernel memory: 340K (80e52000 - 80ea7000)

SELinux:  Permission attach_queue in class tun_socket not defined in policy.

SELinux: the above unknown classes and permissions will be denied

type=1403 audit(1.760:2): policy loaded auid=4294967295 ses=4294967295

SELinux: Loaded policy from /sepolicy

type=1404 audit(1.780:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295

init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.

init: /dev/hw_random not found

keychord: using input dev gpio-keys.27 for fevent

init: cannot open '/initlogo.rle'

Console: switching to colour dummy device 80x30

EXT4-fs (mmcblk3p5): mounted filesystem with ordered data mode. Opts: (null)

EXT4-fs (mmcblk3p4): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk3p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic

EXT4-fs (mmcblk3p6): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk3p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit

EXT4-fs (mmcblk3p7): mounted filesystem with ordered data mode. Opts: (null)

init: /dev/hw_random not found

rfkill: BT RF going to : off

init: cannot find '/system/bin/sh', disabling 'console'

type=1400 audit(4.600:4): avc:  denied  { entrypoint } for  pid=153 comm="init" path="/sbin/healthd" dev="rootfs" ino=152 scontext=u:r:healthd:s0 tcontext=u:object_r:rootfs:s0 tclass=file permissive=1

healthd: BatteryTemperaturePath not found

healthd: BatteryTechnologyPath not found

binder: 153:153 transaction failed 29189, size 0-0

init: cannot find '/system/bin/servicemanager', disabling 'servicemanager'

init: cannot find '/system/bin/vold', disabling 'vold'

init: cannot find '/system/bin/netd', disabling 'netd'

init: cannot find '/system/bin/debuggerd', disabling 'debuggerd'

init: cannot find '/system/bin/surfaceflinger', disabling 'surfaceflinger'

init: cannot find '/system/bin/app_process', disabling 'zygote'

init: cannot find '/system/bin/drmserver', disabling 'drm'

init: cannot find '/system/bin/mediaserver', disabling 'media'

init: cannot find '/system/bin/installd', disabling 'installd'

init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'

init: cannot find '/system/bin/keystore', disabling 'keystore'

init: cannot find '/system/bin/rild', disabling 'ril-daemon'

init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead

init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead

init: property 'ro.product.manufacturer' doesn't exist while expanding '$ro.product.manufacturer'

init: cannot expand '$ro.product.manufacturer' while writing to '/sys/class/android_usb/android0/iManufacturer'

init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead

init: property 'ro.product.model' doesn't exist while expanding '$ro.product.model'

init: cannot expand '$ro.product.model' while writing to '/sys/class/android_usb/android0/iProduct'

init: cannot find '/system/bin/sh', disabling 'wifi_mac'

init: cannot find '/system/bin/sdcard', disabling 'sdcard'

init: cannot find '/system/bin/magd', disabling 'magd'

init: cannot find '/system/bin/ingsvcd', disabling 'ing'

init: property 'sys.powerctl' doesn't exist while expanding '${sys.powerctl}'

init: powerctl: cannot expand '${sys.powerctl}'

init: property 'sys.sysctl.extra_free_kbytes' doesn't exist while expanding '${sys.sysctl.extra_free_kbytes}'

init: cannot expand '${sys.sysctl.extra_free_kbytes}' while writing to '/proc/sys/vm/extra_free_kbytes'

android_usb: already disabled

mtp_bind_config

binder: 153:153 transaction failed 29189, size 0-0

binder: 153:153 transaction failed 29189, size 0-0

binder: 153:153 transaction failed 29189, size 0-0

binder: 153:153 transaction failed 29189, size 0-0

binder: 153:153 transaction failed 29189, size 0-0

binder: 153:153 transaction failed 29189, size 0-0

binder: 153:153 transaction failed 29189, size 0-0

binder: 153:153 transaction failed 29189, size 0-0

binder: 153:153 transaction failed 29189, size 0-0

I could see only ANDROID name on the HDMI Display after it's not showing anything.

Any suggestions please.

Thanks,

Raj.

Regards,
Thanaraj Subramani
标签 (1)
10 回复数

1,889 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Raj,

Were you able to make it work?, I assume your problem is only when using the script but not mfg tools, is that correct?

0 项奖励
回复

1,889 次查看
feifeihu
Contributor II

init: cannot find '/system/bin/servicemanager', disabling 'servicemanager'

init: cannot find '/system/bin/vold', disabling 'vold'

init: cannot find '/system/bin/netd', disabling 'netd'

init: cannot find '/system/bin/debuggerd', disabling 'debuggerd'

init: cannot find '/system/bin/surfaceflinger', disabling 'surfaceflinger'

init: cannot find '/system/bin/app_process', disabling 'zygote'

init: cannot find '/system/bin/drmserver', disabling 'drm'

init: cannot find '/system/bin/mediaserver', disabling 'media'

these means system image is not flashed correctly.

1,889 次查看
caiopereira
Contributor III

I'm having the same problem but with Android 6.0.1 IMX6SABRE SD Dualite

1,889 次查看
BiyongSUN
NXP Employee
NXP Employee

Have you  used mfg tool to try?

and the partition layout in Android is differenct now.

In Android 6.0, the system partition is about 800M.

In Android 6.0, the system.img need simg2img to convert.

If you didn't use mfg tool, did you use the "simg2img" to convert the image?

Android_User's_Guide.pdf

Untitled.png

0 项奖励
回复

1,889 次查看
gary_bisson
Senior Contributor III

Hi BiyongSUN​,

I'm actually wondering why the documentation says 800MB whereas the source code sets it to 600MB? (see device/fsl/imx6/BoardConfigCommon.mk line 84). Also the commit says it changes the sparse image size but BOARD_SYSTEMIMAGE_PARTITION_SIZE changes the raw image size, not the sparse one.

Finally, the flashing script provided in the device folder (device/fsl/common/tools/fsl-sdcard-partition.sh) as well as the script provided in the MFG tool still sets the system partition to 512MB which seems very unlikely to work.

Please clarify.

Regards,

Gary

0 项奖励
回复

1,889 次查看
BiyongSUN
NXP Employee
NXP Employee

Here is the souce code of Android 6.0

android-m6.0.1-1.0.0-ga/device/fsl/imx6/BoardConfigCommon.mk

78 # comment out for 1g/3g space split

79 # TARGET_KERNEL_2G := true

80

81 BOARD_BOOTIMAGE_PARTITION_SIZE := 16777216

82 BOARD_RECOVERYIMAGE_PARTITION_SIZE := 16777216

83

84 BOARD_SYSTEMIMAGE_PARTITION_SIZE := 629145600

85 BOARD_CACHEIMAGE_PARTITION_SIZE := 444596224

86 BOARD_FLASH_BLOCK_SIZE := 4096

87 TARGET_RECOVERY_UI_LIB := librecovery_ui_imx

88

89 # Freescale multimedia parser related prop setting

If you have checked the mksdcard-android.sh in android_m6.0.1_1.0.0_ga_tool\Profiles\Linux\OS Firmware\mksdcard-android.sh.tar

you will see SYSTEM_ROM_SIZE=800.

So far, in the Android 6.0, the system.img is about 526M.

after using simg2img, it is about 629M. 

That is mininal size needed, so leave more space set the patition to 800M.

526867648 Mar 14 15:59 system.img

629108736 May 25 16:32 system_raw.img

#!/bin/bash

# partition size in MB
BOOTLOAD_RESERVE=8
BOOT_ROM_SIZE=16
SYSTEM_ROM_SIZE=800
CACHE_SIZE=512
RECOVERY_ROM_SIZE=16
DEVICE_SIZE=8
MISC_SIZE=6
DATAFOOTER_SIZE=2

help() {

bn=`basename $0`
cat << EOF
usage $bn <option> device_node

options:
  -h    displays this help message
  -s    only get partition size
  -np     not partition.
  -f soc_name   flash android image.
EOF

}

# parse command line
moreoptions=1
node="na"
soc_name=""
cal_only=0
flash_images=0

0 项奖励
回复

1,889 次查看
sumanthg
Contributor II

Hi Biyong Sun,

what is DEVICE_SIZE = 8 specified to ? and what it is used for ? 

#!/bin/bash

# partition size in MB
BOOTLOAD_RESERVE=8
BOOT_ROM_SIZE=16
SYSTEM_ROM_SIZE=800
CACHE_SIZE=512
RECOVERY_ROM_SIZE=16
DEVICE_SIZE=8
MISC_SIZE=6
DATAFOOTER_SIZE=2

help() {

bn=`basename $0`
cat << EOF
usage $bn <option> device_node

options:
  -h    displays this help message
  -s    only get partition size
  -np     not partition.
  -f soc_name   flash android image.
EOF

}

1,889 次查看
gary_bisson
Senior Contributor III

Hi,

Sorry I must have downloaded the wrong MFG tool package, re-downloaded this one today and it is indeed 800MB.

IMX6_M6.0.1_1.0.0_MFG_TOOL

However the script in the source code is wrong, please update it for next release (device/fsl/common/tools/fsl-sdcard-partition.sh).

Regards,

Gary

0 项奖励
回复

1,889 次查看
BiyongSUN
NXP Employee
NXP Employee

Gray,

800M can hold the 629M system image, what is the problem here.

Even you can make it 2G size for system partition to hold the 629M system image.

800M is partition size. We don't know what to corrct next release.

We use the mfg tool to flash the sabresd baord.

No any problem.

We don't know how to help you.

0 项奖励
回复

1,889 次查看
gary_bisson
Senior Contributor III

Hi,

As I said in my last post, the MFG Tool is fine.

But the script you provide under /device/fsl/ does *not* match the one in MFG tool and sets the partition to 512MB. It is not big deal, we can modify it manually but it might make sense to update it for next release.

Regards,

Gary

0 项奖励
回复