IMX6D and PF0100 for LPDDR2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6D and PF0100 for LPDDR2

跳至解决方案
1,161 次查看
egorrumjantsev
Contributor III

Hello, we want to make board on IMX6Dual with LPDDR2. Right now we are selecting version of PF0100. Is there any reference schematic interfacing IMX6, PMIC and LPDDR2?

WBR,

0 项奖励
回复
1 解答
1,049 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  We do not have design with i.MX6 D/Q LPDDR2 and PF0100, but 

You may use the PF0100 F1  (as for i.MX6 SL EVK).

i.MX 6SoloLite Evaluation Kit|NXP 

Regards,

Yuri.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,049 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  I have sent You scheme, which may be helpful via e-mail.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,049 次查看
egorrumjantsev
Contributor III

Sorry, it was delay...now i received mail.

Thank you for help.

But this schematic does not use PF0100. Could you recommed which OTP we should use for LPDDR2 1.2V and IMX6. dual?

WBR,

0 项奖励
回复
1,050 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  We do not have design with i.MX6 D/Q LPDDR2 and PF0100, but 

You may use the PF0100 F1  (as for i.MX6 SL EVK).

i.MX 6SoloLite Evaluation Kit|NXP 

Regards,

Yuri.

0 项奖励
回复
1,049 次查看
egorrumjantsev
Contributor III

Thank you Yuri.

We will try to design board according your recomendations. We did board with IMX6SL, so hope with Dual core we won't have problems.

WBR,

0 项奖励
回复
1,048 次查看
egorrumjantsev
Contributor III

Hello Yuri

Thanks for your answer, but i didn't receive anything via mail. May be spam filters or something else. Could you share it on Google drive, Yandex disk or similar?

WBR,

0 项奖励
回复