IMX6D and PF0100 for LPDDR2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6D and PF0100 for LPDDR2

Jump to solution
1,160 Views
egorrumjantsev
Contributor III

Hello, we want to make board on IMX6Dual with LPDDR2. Right now we are selecting version of PF0100. Is there any reference schematic interfacing IMX6, PMIC and LPDDR2?

WBR,

0 Kudos
Reply
1 Solution
1,048 Views
Yuri
NXP Employee
NXP Employee

Hello,

  We do not have design with i.MX6 D/Q LPDDR2 and PF0100, but 

You may use the PF0100 F1  (as for i.MX6 SL EVK).

i.MX 6SoloLite Evaluation Kit|NXP 

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
5 Replies
1,048 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I have sent You scheme, which may be helpful via e-mail.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,048 Views
egorrumjantsev
Contributor III

Sorry, it was delay...now i received mail.

Thank you for help.

But this schematic does not use PF0100. Could you recommed which OTP we should use for LPDDR2 1.2V and IMX6. dual?

WBR,

0 Kudos
Reply
1,049 Views
Yuri
NXP Employee
NXP Employee

Hello,

  We do not have design with i.MX6 D/Q LPDDR2 and PF0100, but 

You may use the PF0100 F1  (as for i.MX6 SL EVK).

i.MX 6SoloLite Evaluation Kit|NXP 

Regards,

Yuri.

0 Kudos
Reply
1,048 Views
egorrumjantsev
Contributor III

Thank you Yuri.

We will try to design board according your recomendations. We did board with IMX6SL, so hope with Dual core we won't have problems.

WBR,

0 Kudos
Reply
1,047 Views
egorrumjantsev
Contributor III

Hello Yuri

Thanks for your answer, but i didn't receive anything via mail. May be spam filters or something else. Could you share it on Google drive, Yandex disk or similar?

WBR,

0 Kudos
Reply