Hi anny
you are right: they can be connected directly.
EVK board was designed to provide as much possible connections
as possible to test all available interfaces and its options.
These buffers were added for flexibility, for example MX28 EVK board supports
up to 4 NAND flash ICs (CE0, CE1, CE2, and CE3).
However, the 0 ohm options for CE2 and CE3 are disconnected by
default (they are used for CAN).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi anny
you are right: they can be connected directly.
EVK board was designed to provide as much possible connections
as possible to test all available interfaces and its options.
These buffers were added for flexibility, for example MX28 EVK board supports
up to 4 NAND flash ICs (CE0, CE1, CE2, and CE3).
However, the 0 ohm options for CE2 and CE3 are disconnected by
default (they are used for CAN).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The Buffers are used as level shifter (3.3V to 5V and 5V to 3.3V) if You use a 3.3V CAN-Bus Transceiver (for example SN65HVD232 from TI) they are not needed, or if You use a 5V type with TTL Inputs, You only have to reduce the RX output to 3.3V level .
Martin