Hello all:
The correction DDR is normal on the common board, but abnormal below appears on my own board correction
Press Download button and to appear as shown below
I'm sure my board is in download mode,also A “HID-compliant device” or “USB Input Device” will be shown in the Device Manager as Figure
What should I do?
Hi
usage and description of ddr test can be found in MSCALE_DDR_Tool_User_Guide.pdf
document included in test package found on
https://community.nxp.com/docs/DOC-340179
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor:
I have a DDR of the same model with different memory, now 3G and 4G can be corrected, when I press Calibration to do DDR Training 1G and 2G will have the following error, why? I use the same one DDR script (DS file)
you should create special DDR script (DS file) for used memory using
MX8M_LPDDR4_RPA_v23.xlsx tool from link:
i.MX8 MSCALE SERIES DDR Tool Release (V2.10)
then follow p.9 sect.4. Load DDR initialization script and choose correct downloading options
MSCALE_DDR_Tool_User_Guide.pdf
Best regards
igor
Hi igor ;
When I did the stress test it showed this fail,
LPDDR4 memory (MT 53 B 512M32 D2) ;How to modify DS file?
Do you have the 2GB LPDDR4 script?