i.MX wit NAND Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX wit NAND Flash

2,037 Views
jupiter_hce
Contributor III

Hi,

Has anyone use NAND for iMX6?  Appreciate advice to work with NAND.

Thank you.

- JH

Drive your NAND within Linux Forget the word "nightmare" - YouTube 

0 Kudos
Reply
3 Replies

1,911 Views
igorpadykov
NXP Employee
NXP Employee

Hi jupiter

yes nand can be used with i.MX6, one can look on NXP Linux documentation
i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,911 Views
jupiter_hce
Contributor III

Thanks igor, I am using i.MX 6ULZ processor (MCIMX6Z0DVM09AB) with internal NAND flash for a customized board, will it be sufficient to config UBOOT_CONFIG = "nand" in local.conf for downloading Linux kernel image to NAND and boot from NAND? I am also using the imx mfgtool uuu, do I need to configure UBOOT_CONFIG["mfgtool]?

Thank you very much.

Kind regards,

- jupiter

0 Kudos
Reply

1,911 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply