I210 Ethernet Support for IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I210 Ethernet Support for IMX6

1,570 Views
ashokp
Contributor I

Hi All,

I am adding the support for I210 intel Ethernet controller support in IMX6 Yocto based BSP. The kernel version is 3.10.31 with device tree support. The I210 device is a PCIe based device. Please let me know if any changes required in dts file to add the support for i210 Ethernet controller. 

Thanks,

P.Ashok

0 Kudos
Reply
1 Reply

842 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ashok

i.MX6 PCIe interface is standard inteface, not requiring

additional reconfiguration for every PCIe device, so no need for

changes in dts file.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply