I

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
730 Views
cyrusvali
Contributor II

Hi

I have a question about ARM architecture

why there is two registers to enable/disable interrupts? ISER and ICER

Is it not possible to set/reset the same register for enable/disabling the interrupts?

thank you

1 Solution
623 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Cyrus,

this question is related to ARM Cortex processor rather that the whole NXP MCU. For instance you should identify which ARM core are you using. For details about ARM cores you may contact ARM or check their infocenter.

4.2.3. Interrupt Clear-enable Register

4.2.2. Interrupt Set-enable Registers


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
624 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Cyrus,

this question is related to ARM Cortex processor rather that the whole NXP MCU. For instance you should identify which ARM core are you using. For details about ARM cores you may contact ARM or check their infocenter.

4.2.3. Interrupt Clear-enable Register

4.2.2. Interrupt Set-enable Registers


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------