Hello,
1) When the GPIO pins are configured as output pins, what is the output type? Can we choose between push pull and open drain? I couldn't find this information in the datasheet.
2) I have to use a level shifter for the GPIO pins. Would you see an issue with using: http://www.ti.com/product/TXS0108E?dcmp=dsproject&hqs=pf?
Thank you,
Faiz
Hello,
1.
IMX8Mm output pins can be configured as CMOS or as open drain, using corresponding
Pad Control Register.
2.
Customers can use the mentioned shifter.
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------