I.MX8 Mini gpio pins output type?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX8 Mini gpio pins output type?

568件の閲覧回数
faiz
Contributor I

Hello,

1) When the GPIO pins are configured as output pins, what is the output type? Can we choose between push pull and open drain? I couldn't find this information in the datasheet.

2) I have to use a level shifter for the GPIO pins. Would you see an issue with using: http://www.ti.com/product/TXS0108E?dcmp=dsproject&hqs=pf?

Thank you,

Faiz

0 件の賞賛
1 返信

472件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

1.

  IMX8Mm output pins can be configured as CMOS or as open drain, using corresponding

Pad Control Register.  

2.

  Customers can use the mentioned shifter.


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛