I.MX6 SoloX hardware accelerated codec sample code (for h.264 encoding/decoding)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.MX6 SoloX hardware accelerated codec sample code (for h.264 encoding/decoding)?

1,767 次查看
ioancalapod
Contributor II

Where can I find hardware accelerated codec sample code (for h.264 encoding/decoding) for I.MX SoloX?

标签 (1)
0 项奖励
回复
4 回复数

1,366 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ioan

i.MX6SX has not vpu module, so video codec can be implemeneted

only in software.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,366 次查看
ioancalapod
Contributor II

Igor

Understood.

Where do I find that kind of code (H.264 - SW encoding decoding )?

Best Regards, Ioan

0 项奖励
回复

1,366 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ioan

please check attached Release Notes Table 23. Video codec specification for hardware

without VPU acceleration and Linux Manual from Doc package

Board Support Packages (27)

L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

meta-fsl-arm/recipes-multimedia/libfslcodec at master · Freescale/meta-fsl-arm · GitHub

Best regards

igor

0 项奖励
回复

1,366 次查看
ioancalapod
Contributor II

Thanks Igor.

Much appreciated.

Best Regards, Ioan

Ioan Calapod, Eng.

Field Application Engineer

Arrow Electronics Montreal

1425 Trans Canada Highway, Suite 140

Dorval, Quebec H9P 2W9

Mobile: (514) 730-5766

Direct: (514) 421-4384

Email: icalapod@arrow.com<mailto:icalapod@arrow.com>

Look for parts at: http://parts.arrow.com/

0 项奖励
回复