I.MX6 - H.264 encoding of Framebuffer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.MX6 - H.264 encoding of Framebuffer

3,035 次查看
anoopaugustine
Contributor II

Hi, I am trying to H.264 encode the framebuffer in i.MX6Q. My requirement is to encode and stream the framebuffer. I am able to open /dev/fb0 and grab the frame. I understand from the H.26 encoder requirements that t operates only on YUV frames. I am trying color space conversion of RGB framebuffer using IPU and then encoding using the VPU. But all these operations takes more than 100ms which I am not able to afford. Could you please suggest me a better way to do this? Is there a way I can configure /dev/fb0 for YUV and H.264 encoder can directly operate on framebuffer memory? Is there any samples available?

9 回复数

2,227 次查看
anoopaugustine
Contributor II

Hi Igor,

Thanks for the response.

I am using the following encode and decode example code.
https://github.com/Freescale/libimxvpuapi/blob/master/example/encode-example.c
https://github.com/Freescale/libimxvpuapi/blob/master/example/decode-example.c

I am trying to H264 encode a single frame (1920 * 1080 in I420 format). Encoding is succeeded using the encode example (I have updated frame width and height as 1920* 1080 in the example code). But while decoding using decode example I get following error and it is not producing decoded image file. What could be the problem here? Is it not possible to decode a single frame.

  [INFO]  bitstreamMode 1, chromaInterleave 0, mapType 0, tiled2LinearEnable 0
encoded input frame:  frame id: 0x64  size: 320710 byte
initial info:  size: 1920x1088 pixel  rate: 4294967295/4294967295  min num required framebuffers: 8  interlacing: 0  framebuffer alignment: 1
calculated sizes:  frame width&height: 1920x1088  Y stride: 1920  CbCr stride: 960  Y size: 2088960  CbCr size: 522240  MvCol size: 522240  total size: 3655681
draining decoder
VPU reports EOS; no more decoded frames available

Thanks & Regards

Anoop

0 项奖励
回复

2,227 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Anoop

libimxvpuapi is community api, please post its issues on

meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale

also one can look at vpu examples in unit tests

imx-test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor

2,227 次查看
anoopaugustine
Contributor II

Hi Igor,

Thanks for your support.

I tried out the VPU H.264 unit test. I am seeing  ~30fps for encoding 1920*1080 frame. But for decoding it is showing fps as ~6fps. It takes about 162ms for decoding a single frame. That is way too slow. What could be the issue?

root@imx6qsabreauto:/unit_tests# ./mxc_vpu_test.out -E "-i /home/root/converted.yuv -f 2 -a 25 -o te...
[INFO]    VPU test program built on Jun 19 2017 11:13:06
[INFO]    Product Info: i.MX6Q/D/S
[INFO]    VPU firmware version: 3.1.1_r46072
[INFO]    VPU library version: 5.4.35
[INFO]    Format: STD_AVC
[INFO]    AVC
[INFO]    Input file "/home/root/converted.yuv" opened.
[INFO]    Output file "test1.h264" opened.
[INFO]    Capture/Encode fps will be 25
[INFO]    ringBufferEnable 0, chromaInterleave 1, mapType 0, linear2TiledEnable 0
[INFO]    Finished encoding: 1 frames
[INFO]    enc fps = 44.92
[INFO]    total fps= 30.77

root@imx6qsabreauto:/unit_tests# ./mxc_vpu_test.out -D "-i test1.h264 -f 2 -a 25 -o test1.yuv -w 1920 -h 1080"
[INFO]    VPU test program built on Jun 19 2017 11:13:06
[INFO]    Product Info: i.MX6Q/D/S
[INFO]    VPU firmware version: 3.1.1_r46072
[INFO]    VPU library version: 5.4.35
[INFO]    Format: STD_AVC
[INFO]    AVC
[INFO]    Input file "test1.h264" opened.
[INFO]    Output file "test1.yuv" opened.
[INFO]    bitstreamMode 1, chromaInterleave 1, mapType 0, tiled2LinearEnable 0
[INFO]    H.264 Profile: 66 Level: 40 Interlace: 0
[INFO]    sar_width: 65535, sar_height: 65535
[INFO]    Decoder: width = 1920, height = 1088, frameRateRes = 4294967295, frameRateDiv = 4294967295, count = 3
[INFO]    CROP left/top/right/bottom 0 0 1920 1080
[INFO]    1 frames took 162439 microseconds
[INFO]    dec fps = 64.28
[INFO]    total fps= 6.16
Thanks & Regards
Anoop
0 项奖励
回复

2,227 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Anoop

please try Demo Images on i.MX6Q Sabre AI board

http://www.nxp.com/webapp/Download?colCode=IMX6_N7.1.1_1.0.0_ANDROID_DEMO_AI_BSP&appType=license&loc... 

Best regards
igor

0 项奖励
回复

2,227 次查看
anoopaugustine
Contributor II

Hi Igor,

Thanks for the quick response!. I have referred mxc_vpu_test application. I would like to know if /dev/fb0 can be configured for YUV color space and I can use this framebuffer directly for H.264 encoding.

Thanks & Regards

Anoop

0 项奖励
回复

2,227 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Anoop

data for encoding may be feed also from framebuffer, one can use

(if necessary) color conversion using examples on

https://community.freescale.com/docs/DOC-94961

Best regards
igor

2,227 次查看
anoopaugustine
Contributor II

Hi Igor,

Thanks for the examples.

I tried to change the VPU clock frequency to MX6_VPU_352M in menuconfig to improve performance. But after setting this the encoder performance is lowered. Is there any other configuration that I need to do for changing VPU clock?

Thanks & Regards

Anoop

2,227 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Anoop

please check VDD_SOC voltage for 352MHz operation

described in Table 6. Operating Ranges i.MX6DQ Reference Manual
http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf

Best regards
igor

0 项奖励
回复

2,227 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Anoop

please check examples in unit tests (..test/mxc_vpu_test)

imx-test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------