I followed the guide of vprovfiler,
USE_POWER_MANAGEMENT = 0
USE_PROFILER = 1
But when I execute the open GLES application, the application crashed, and failure log is: segmentation fault!
Please clarify which release are you using?
Which backend are you using?
And which application are you using for test?
Thanks.
The kernel verison : 3.0.35 from L3.0.35_4.0.0_130424_source
Backend :
Test application : tutorial1_es20
Are you using default ltib rootfs?
And please double check if your vdk version is 1.4.5.
Can the Modified kernel co-work is standard rootfs?
Thanks.
Yes, I use the default ltib rootfs, How to get the version of the vdk?
It should be shown at the VDK package name.
Unfortunately, I didn't find the version at the package name, the package is downloaded from https://www.freescale.com/webapp/Download?colCode=I.MX_6DL_S_VIVANTE_VDK_TOOLS&appType=license&locat... and our soc is imx6solo.
In the package, it shows the vdk tools is for 3.0.0 release. "Linux L3.0.35_3.0.0 GPU Driver with vprofiler"
Please use the correct vdk tool package for 4.0.0 release.
Hello,
I have the same problem about the vprofiler , when I execute the openGLES application (opt/viv_samples/vdk), the application crashed : segmentation fault :smileyblush:
Have you got a tarball of system with the integrated profiler ?
Regards,
It should be vtk package.
Hi ,
I downloaded the Kernel 3.0.35 adn the VDK tools from i.MX 6 Q/D/DL/S L3.0.35_4.1.0 GA release .
After that I modified the configure file of GPU driver:-
USE_POWER_MANAGEMENT = 0
USE_PROFILER = 1
Then i extracted the pre-built binaries (enable the profile) and replace the libraries.
Then as mentioned in the readme file executed the ./ltib command to build.
But now when i am running any OpeGLES application I am getting a Segmentation Fault.
Can somebody please help here?