How to use the VIV GPU vprovfiler?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the VIV GPU vprovfiler?

5,423 Views
liangluo
Contributor II

I followed the guide of vprovfiler,

  • modify the configure file of GPU driver.

          USE_POWER_MANAGEMENT = 0

          USE_PROFILER                       = 1

  • Extract the pre-built binaries (enable the profile) and replace the libraries

But when I execute the open GLES application, the application crashed, and failure log is: segmentation fault!

Labels (3)
10 Replies

4,276 Views
LorenHuang
Contributor IV

Please clarify which release are you using?

Which backend are you using?

And which application are you using for test?

Thanks.

0 Kudos
Reply

4,276 Views
liangluo
Contributor II

The kernel verison : 3.0.35 from L3.0.35_4.0.0_130424_source

Backend :

Test application : tutorial1_es20

0 Kudos
Reply

4,276 Views
LorenHuang
Contributor IV

Are you using default ltib rootfs?

And please double check if your vdk version is 1.4.5.

Can the Modified kernel co-work is standard rootfs?

Thanks.

0 Kudos
Reply

4,276 Views
liangluo
Contributor II

Yes, I use the default ltib rootfs, How to get the version of the vdk?

0 Kudos
Reply

4,276 Views
LorenHuang
Contributor IV

It should be shown at the VDK package name.

4,276 Views
liangluo
Contributor II

Unfortunately, I didn't find the version at the package name, the package is downloaded from https://www.freescale.com/webapp/Download?colCode=I.MX_6DL_S_VIVANTE_VDK_TOOLS&appType=license&locat... and our soc is imx6solo.

0 Kudos
Reply

4,276 Views
LorenHuang
Contributor IV

In the package, it shows the vdk tools is for 3.0.0 release. "Linux L3.0.35_3.0.0 GPU Driver with vprofiler"

Please use the correct vdk tool package for 4.0.0 release.

0 Kudos
Reply

4,276 Views
texierp
Contributor III

Hello,

I have the same problem about the vprofiler , when I execute the openGLES application (opt/viv_samples/vdk), the application crashed : segmentation fault :smileyblush:

  • I use Kernel 3.0.35 from L3.0.35_4.1.0_130816_source (LTIB).
  • My board = imx6 sabrelite

Have you got a tarball of system with the integrated profiler ?

Regards,

0 Kudos
Reply

4,276 Views
LorenHuang
Contributor IV

It should be vtk package.

0 Kudos
Reply

4,276 Views
puneetpalsingh
NXP Employee
NXP Employee

Hi ,

I downloaded the Kernel 3.0.35 adn the VDK tools from i.MX 6 Q/D/DL/S L3.0.35_4.1.0 GA release .

After that I modified the configure file of GPU driver:-

USE_POWER_MANAGEMENT = 0

USE_PROFILER                       = 1

Then i extracted the pre-built binaries (enable the profile) and replace the libraries.

Then as mentioned in the readme file executed the ./ltib command to build.


But now when i am running any OpeGLES application I am getting a Segmentation Fault.


Can somebody please help here?

0 Kudos
Reply