Hi ,
I used iMX6 in my project, I want to use Flexray and choice MFR4310+ TJA1080, but MFR4310 is using Asynchronous Memory Interface.
How to connect MFR4310 to iMX6? If it can not to do, which the solution of Flexray is good?
B.R
Ben
Hello Wang,
The only way that I see to interface it, it is using the EIM interface, just like it shows the reference manual of the MFR4310 in the figure 2.7. MPC Interface with MPC5xx and MPC5xxx Families.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------