How to partition the flash to support Encrypted XiP and filesystem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to partition the flash to support Encrypted XiP and filesystem

486 Views
Hariprasath_K
Contributor I

We are studying i.MXRT1172 processor to be used in our product.
We need encrypted XiP feature and also a filesystem partition to store the resources (log file, UI resources, etc.). We have decided to use MQX OS. We have decided to keep an external flash (QSPI interface).

For the above requirement we have designed the flash layout as shown in below picture,

Hariprasath_K_1-1661165882082.png

Now the question, is it possible to use a single flash memory chip to keep the application binaries and a partition for the filesystem like shown in above image?

0 Kudos
Reply
1 Reply

473 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Yes, that would be possible, with and without RTOS.

 

You can also check with the MQX support for that (once you buy mqx)

 

Regards

Vicente Gomez

0 Kudos
Reply