I am evaluating the Sabre SD board with a PCIe switch, and I am having issues getting it to work in Gen 2 mode.
This is using the Linux kernel 3.0.35-4.0.0 BSP.
I would like to force it into Gen 1 mode for testing, and this patch has worked to get it going for initial bring up.
===========================================================================
--- patched-linux-3.0.35-imx/arch/arm/mach-mx6/pcie.c 2013-09-26 14:49:46.000000000 -0700
+++ linux-3.0.35-imx/arch/arm/mach-mx6/pcie.c 2013-09-26 15:37:49.720701981 -0700
@@ -1021,8 +1021,13 @@ static int __devinit imx_pcie_pltfm_prob
if (!(pdata->type_ep)) {
/*Only RC: togle the external card's reset */
card_reset(dev) ;
+ usleep_range(4000, 5000);
imx_pcie_regions_setup(dev, dbi_base);
+ usleep_range(4000, 5000);
+ /* Force GEN1 */
+ writel(((readl(dbi_base + LNK_CAP) & 0xfffffff0) | 0x1), dbi_base + LNK_CAP);
+ usleep_range(4000, 5000);
}
pr_info("PCIE: %s start link up.\n", __func__);
===========================================================================
However, now I am testing suspend to RAM, and I am having problems getting it working. Is there a recommended way I can force it to Gen1 that will survive a suspend/resume cycle? Note that I have applied the L2 reset patch and I am able to successfully suspend/resume using an e1000e based card. I have tried rewriting the LNK_CAP register after coming out of suspend but it does not seem to have any effect. I am thinking that I'm simply not setting it at the correct time, and hope that someone can suggest where it should go.
解決済! 解決策の投稿を見る。
Hi:
I used to reply this customer's question by "PCIe imx6 switch issue continuation of SR 1-1159433048" , here is details.
At my side, I used the codes listed below too.
+ /* Force GEN1 */
+ writel(((readl(dbi_base + LNK_CAP) & 0xfffffff0) | 0x1), dbi_base + LNK_CAP);
+ usleep_range(4000, 5000);
My tests:
Because I don’t have PLX8603 switch, I just used the i.MX6Q SD + GEN2 PCIe EP device(usb3.0 xhci device)
to do the suspend/resume tests when the link_cap of PCIe RC(i.MX6Q SD) is limited to PCIe GEN1 speed.
Before suspend:
root@freescale ~$ lspci -vv
00:00.0 PCI bridge: Unknown device 16c3:abcd (rev 01) (prog-if 00 [Normal decode])
...
Device: MaxPayload 128 bytes, MaxReadReq 512 bytes
Link: Supported Speed 2.5Gb/s, Width x1, ASPM L0s L1, Port 0
Link: Latency L0s <1us, L1 <8us
After resume back:
root@freescale ~$ lspci -vv
00:00.0 PCI bridge: Unknown device 16c3:abcd (rev 01) (prog-if 00 [Normal decode])
...
Link: ASPM Disabled RCB 64 bytes CommClk- ExtSynch-
Link: Speed 2.5Gb/s, Width x1
Root: Correctable- Non-Fatal- Fatal- PME-
...
The ‘Max_Link_Speeds’ of 0x7c LNK_CAP is always 1 after out of the suspend.
root@freescale ~$ ./memtool -32 01ffc000 40
Reading 0x80 count starting at address 0x01FFC000
0x01FFC000: ABCD16C3 00100147 06040001 00010010
0x01FFC010: 01000000 00000000 00010100 000000F0
0x01FFC020: 01100110 0000FFF0 00000000 00000000
0x01FFC030: 00000000 00000040 00000000 0001019B
0x01FFC040: DBC35001 00000000 00000000 00000000
0x01FFC050: 01807005 00000000 00000000 00000000
0x01FFC060: 00000000 00000000 00000000 00000000
0x01FFC070: 00420010 00008000 00102010 0011CC11
Regarding to your description, it seems that the LNK_CAP is changed, right?
So I suggest customer that
"can you debug into the code, and make a check when LNK_CAP is changed?"
BTW, attached the email.
Best Regards
Richard
Alex, please click Correct Answer/Helpful Answer, if your question has been answered.
Thanks,
Yixing
Hi:
I used to reply this customer's question by "PCIe imx6 switch issue continuation of SR 1-1159433048" , here is details.
At my side, I used the codes listed below too.
+ /* Force GEN1 */
+ writel(((readl(dbi_base + LNK_CAP) & 0xfffffff0) | 0x1), dbi_base + LNK_CAP);
+ usleep_range(4000, 5000);
My tests:
Because I don’t have PLX8603 switch, I just used the i.MX6Q SD + GEN2 PCIe EP device(usb3.0 xhci device)
to do the suspend/resume tests when the link_cap of PCIe RC(i.MX6Q SD) is limited to PCIe GEN1 speed.
Before suspend:
root@freescale ~$ lspci -vv
00:00.0 PCI bridge: Unknown device 16c3:abcd (rev 01) (prog-if 00 [Normal decode])
...
Device: MaxPayload 128 bytes, MaxReadReq 512 bytes
Link: Supported Speed 2.5Gb/s, Width x1, ASPM L0s L1, Port 0
Link: Latency L0s <1us, L1 <8us
After resume back:
root@freescale ~$ lspci -vv
00:00.0 PCI bridge: Unknown device 16c3:abcd (rev 01) (prog-if 00 [Normal decode])
...
Link: ASPM Disabled RCB 64 bytes CommClk- ExtSynch-
Link: Speed 2.5Gb/s, Width x1
Root: Correctable- Non-Fatal- Fatal- PME-
...
The ‘Max_Link_Speeds’ of 0x7c LNK_CAP is always 1 after out of the suspend.
root@freescale ~$ ./memtool -32 01ffc000 40
Reading 0x80 count starting at address 0x01FFC000
0x01FFC000: ABCD16C3 00100147 06040001 00010010
0x01FFC010: 01000000 00000000 00010100 000000F0
0x01FFC020: 01100110 0000FFF0 00000000 00000000
0x01FFC030: 00000000 00000040 00000000 0001019B
0x01FFC040: DBC35001 00000000 00000000 00000000
0x01FFC050: 01807005 00000000 00000000 00000000
0x01FFC060: 00000000 00000000 00000000 00000000
0x01FFC070: 00420010 00008000 00102010 0011CC11
Regarding to your description, it seems that the LNK_CAP is changed, right?
So I suggest customer that
"can you debug into the code, and make a check when LNK_CAP is changed?"
BTW, attached the email.
Best Regards
Richard