Hi NXP
Our OS is Yocto4.0 -5.15.52.
Our platform is imx6q.
The spi pin information:
pinctrl_ecspi1: ecspi1grp {
fsl,pins = <
MX6QDL_PAD_EIM_D17__ECSPI1_MISO 0x100b1
MX6QDL_PAD_EIM_D18__ECSPI1_MOSI 0x100b1
MX6QDL_PAD_EIM_D16__ECSPI1_SCLK 0x100b1
>;
};
cs pin : MX6QDL_PAD_EIM_D19__ECSPI1_SS1
We try to add spi (ECSPI1) BUS 0 ,CS1 in uboot.
The result is "spi_xchg_single: Timeout! "
Do you have example code about add BUS0 ,CS1 SPI for Uboot Yocto 4.0?
or
Do you have example code two spi in Bus0 cs0 / bus0 cs1 for uboot Yocto4.0?
Thanks
I will update to you in the case you create.