How to define jtag chain for imx6 with realview ICE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to define jtag chain for imx6 with realview ICE

Jump to solution
2,252 Views
leeseungik
Contributor III

Any body can help me?

I am following steps to connect to jtag with realview ICE which is mentioned document "Hardware Development Guide for i.MX 6Quad..Families of Applications Processors"

in chapter 6.4 NOTE say at page 71 "go to www.freescale.com to obtain your copy of the Freescale_iMX6 Q.rvs file." to define the JTAG chain for a Cortext-A9 based chip. but I can't find that file

where can I find that file?

Thanks

Seungik Lee

Labels (1)
Tags (4)
1 Solution
1,363 Views
Yuri
NXP Employee
NXP Employee

I found the enclosed in my "…/My Documents\ARM\rvconfig\platformFiles".

View solution in original post

6 Replies
1,364 Views
Yuri
NXP Employee
NXP Employee

I found the enclosed in my "…/My Documents\ARM\rvconfig\platformFiles".

1,363 Views
leeseungik
Contributor III

Thanks Yuri.

that file you attached works fine. I steps up to target connection.

But I faced new stage, When I try to access register mentioned in the Guide. memory access error occurs like following..

"Error: 0x021d0102: Error Memory access caused precise abort.

Debug Precise Abort Registers : DFSR = 0x00000005, DFAR = 0x020E0220 from target : Cortex-A9_3."

0 Kudos
Reply
1,362 Views
Yuri
NXP Employee
NXP Employee

Often it is needed to run an initialization script before i.MX registers access.
Please try proper script from the SDK (tools):

https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null&fpsp=1&WT_TYPE=Sn...

0 Kudos
Reply
1,362 Views
leeseungik
Contributor III

Can you tall me how to run script file on linux ? or realview debugger?

0 Kudos
Reply
1,362 Views
Yuri
NXP Employee
NXP Employee

In the RealView Debugger : Menu Tools -> Include Commands from File

0 Kudos
Reply
1,362 Views
leeseungik
Contributor III

Now I can access to Memory..

When I hold console at u-boot then connect to target , now I can access to memory and run script.

thank you for your reply (so fast reply ^^)

0 Kudos
Reply