How to confirm whether i.MX6SDL ERR007110 or ERR007220 occur.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to confirm whether i.MX6SDL ERR007110 or ERR007220 occur.

跳至解决方案
827 次查看
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6SDL.

Actually, their custom board does not boot from NAND only occasionally, and we doubt ERR007117 and ERR007220.

So we want to confirm whether this boot issue is cause by ERR007117 or ERR007220

Could you let me know how to confirm it?

Best Regards,

Satoshi Shimoda

标签 (2)
0 项奖励
回复
1 解答
717 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

for ERR007117 one can attach jtag and output ENFC_CLK_ROOT

on CLKO pad using register CCM_CCOSR and check signal by oscilloscope.

For ERR007220 oen can add additional FCB records using

sect.8.5.2.2 "NAND Flash Boot Flow and Boot Control Blocks (BCB)"  IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
718 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

for ERR007117 one can attach jtag and output ENFC_CLK_ROOT

on CLKO pad using register CCM_CCOSR and check signal by oscilloscope.

For ERR007220 oen can add additional FCB records using

sect.8.5.2.2 "NAND Flash Boot Flow and Boot Control Blocks (BCB)"  IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复