How to confirm whether i.MX6SDL ERR007110 or ERR007220 occur.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to confirm whether i.MX6SDL ERR007110 or ERR007220 occur.

Jump to solution
789 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6SDL.

Actually, their custom board does not boot from NAND only occasionally, and we doubt ERR007117 and ERR007220.

So we want to confirm whether this boot issue is cause by ERR007117 or ERR007220

Could you let me know how to confirm it?

Best Regards,

Satoshi Shimoda

Labels (2)
0 Kudos
Reply
1 Solution
679 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

for ERR007117 one can attach jtag and output ENFC_CLK_ROOT

on CLKO pad using register CCM_CCOSR and check signal by oscilloscope.

For ERR007220 oen can add additional FCB records using

sect.8.5.2.2 "NAND Flash Boot Flow and Boot Control Blocks (BCB)"  IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
680 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

for ERR007117 one can attach jtag and output ENFC_CLK_ROOT

on CLKO pad using register CCM_CCOSR and check signal by oscilloscope.

For ERR007220 oen can add additional FCB records using

sect.8.5.2.2 "NAND Flash Boot Flow and Boot Control Blocks (BCB)"  IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply