How to build mxc_vpu_test int Linux BSP L3.14.52?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to build mxc_vpu_test int Linux BSP L3.14.52?

1,235 Views
junhuaqiao
Contributor III

Hi all

  I want to do a VPU test on iMX6Q plus, use Linux BSP 3.14.52. 

  I tried to build mxc_vpu_test but failed.

  Where can I find the file mxc_ipu_hl_lib.h ?

Thanks,

Qiao

Labels (1)
0 Kudos
Reply
1 Reply

683 Views
igorpadykov
NXP Employee
NXP Employee

Hi Qiao

attached is mxc_ipu_hl_lib.h and for build one can look at imx-test: Upgrade to 5.3 version

[meta-fsl-arm,16/27] imx-test: Upgrade to 5.3 version - Patchwork

i.MX6QP will be supported in unified linux release after 23Feb.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply