How to add kernel parameter?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add kernel parameter?

Jump to solution
3,766 Views
nguyentuan_k58h
Contributor II

Hi experts,

I want to use the on-chip board Wifi QCA6174 of IMX8M Quad Evk Kit. I'm using yocto to build my distro fsl-imx-xwayland, kernel 4.9.88-2.0.0 (rocko)

Following release notes document "For i.MX 8MQuad, it needs to add kernel parameter
"pci=nomsi" to support Murata 1CQ Wi-Fi". But i didn't find the way to add it. 

Can you tell me how I can solve this problem and the steps for using the wlan chip QCA6174? Thank you.

Best regards,

1 Solution
6 Replies
3,564 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tuan

this is general linux parameter and one can try to use it in the same way as

described in Table 10. Common kernel boot parameters. QCA6174 is described in

sect.4.12 Wi-Fi QCA6174 Linux Manual in Linux 4.9.88_2.0.0 BSP & Multimedia Codecs Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,564 Views
nguyentuan_k58h
Contributor II

Hi igor,

I still can not figure out how to add kernel parameter.

I have try modprobe kernel.pci=nomsi but it did not work.

Btw, where is QCA6174 driver located in /lib/firmware/.

0 Kudos
Reply
3,565 Views
igorpadykov
NXP Employee
NXP Employee
3,564 Views
nguyentuan_k58h
Contributor II

Hi igorpadykov

I've tried your solution in version L5.4.3_1.0.0 . It did not work. the interface wlp1s0 was not shown.

I've read release note of this version, there no guide to enable onchip wifi.

Can you tell me how to enable onchip wifi in version L5.4.3_1.0.0?

0 Kudos
Reply
3,564 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tuan

one can try to follow sect.4.13.7 Configuring WLAN from User Space

Linux Manual included in Linux 5.4.3_1.0.0 Documentation

Best regards
igor

0 Kudos
Reply
3,564 Views
nguyentuan_k58h
Contributor II

Hi igorpadykov

Here is image which i flashed "https://www.nxp.com/webapp/Download?colCode=L5.4.3_1.0.0_MX8MQ&appType=license "

Actually, i've tried to procedure from "Reference manual" guide. 

When i run "wpa_supplicant -B -i wlp1s0 -c /etc/wpa_supplicant.conf -D nl80211"

Error show "Could not interface wlp1s0 flags: No such device" 

By the way, command "iw dev" show nothing when i hit. 

0 Kudos
Reply