Hi
I want to remove the uboot in order to test how to recover the imx8 board when it's empty .
I am working now with imx8mm evk but I will work with custom board and I pretend that it will come without boot loader and without an image.
Any information will be very helpful.
Best Regards
Houssem
Hello Houssem,
The recovery from SD can not be possible but for complete deletion of the sd card try:
dd if=/dev/zero of=/dev/sdx
where x is your SD.
Then you can program the bootloader.
Regards
Hello Bio
The default bootloader is stored at the ROM and the default image is stored in the emmc.
I have successfully removed the image by using the uboot mmc erase command to but now i want to remove the uboot from the ROM memory.
Best Regards