How Erase uboot from imx8mm evk ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How Erase uboot from imx8mm evk ?

2,512件の閲覧回数
houssem_chaaban
Contributor II

Hi

I want to remove the uboot in order to test how to recover the imx8 board when it's empty .

I am working now with imx8mm evk but I will work with custom board and I pretend that it will come without boot loader and without an image.

Any information will be very helpful.

Best Regards

Houssem

タグ(2)
3 返答(返信)

2,330件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Houssem,

The recovery from SD can not be possible but for complete deletion of the sd card try:

dd if=/dev/zero of=/dev/sdx

where x is your SD.

Then you can program the bootloader.

Regards

0 件の賞賛
返信

2,330件の閲覧回数
houssem_chaaban
Contributor II

Hello Bio


The default bootloader is stored at the ROM and the default image is stored in the emmc.

I have successfully removed the image by using the uboot mmc erase command to but now i want to remove the uboot from the ROM memory.


Best Regards

2,330件の閲覧回数
tdoering
Contributor II

Hi,

any news on this?

Greetings,

Thomas

0 件の賞賛
返信