Hi, I need a reliable statement which Windows 7 driver has to be used when attaching the MCIMX6Q-SDB to the Windows 7 PC via the USB cable (part of the SDB board delivery) where a virtual com port is used. Where can I get hold of that driver?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, I need a reliable statement which Windows 7 driver has to be used when attaching the MCIMX6Q-SDB to the Windows 7 PC via the USB cable (part of the SDB board delivery) where a virtual com port is used. Where can I get hold of that driver?

862 Views
bschild
Contributor I

Indeed, my question sounds very silly. However, I need a reliable answer.

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

608 Views
SergioSolis
NXP Employee
NXP Employee

Well, windows 7 should automatically look for the driver and install it (I haven't seen it fail yet). You need to make sure that your board's boot switches are all in "off" to go to serial mode and then connect the board to the PC and turn it on.

0 Kudos
Reply