Hi, I need a reliable statement which Windows 7 driver has to be used when attaching the MCIMX6Q-SDB to the Windows 7 PC via the USB cable (part of the SDB board delivery) where a virtual com port is used. Where can I get hold of that driver?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi, I need a reliable statement which Windows 7 driver has to be used when attaching the MCIMX6Q-SDB to the Windows 7 PC via the USB cable (part of the SDB board delivery) where a virtual com port is used. Where can I get hold of that driver?

863件の閲覧回数
bschild
Contributor I

Indeed, my question sounds very silly. However, I need a reliable answer.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

609件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Well, windows 7 should automatically look for the driver and install it (I haven't seen it fail yet). You need to make sure that your board's boot switches are all in "off" to go to serial mode and then connect the board to the PC and turn it on.

0 件の賞賛
返信