I have been working with imx6dq custom board , The hdmi to dvi display is connected to hdmi port of imx6 custom board. (based on Sabresd). And booted the board. Now the output of the display is stable.
If i boot the board and hot plug the hdmi to dvi cable to imx6 board. the output data, which is transmitted from the imx6 board is flickering. with the response of the input events (example: crossing the mouse or typing the data from the
The display is flickering continuously, how to resolve the problem?
kernel version : 3.14.52
android flavor : marshmallow
Hello,
Can you please try with our Android BSP 6.0.1_2.1.0? I tested with both BSP, and no one give me the flickering that you are mentioning.
Best Regards,
Diego.
In the below link you can find the download link:
Android OS for i.MX Applications Processors|NXP
You only need to search for the BSP that you are willing to use.
Best Regards,
Diego