HDMI display spash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI display spash

806 Views
1182614726
Contributor III

Hello, now i'm using linux L4.1.15-2.0.0 BSP, and u-boot is 2016-03 version and configure HDMI interface to display. Now i add the patch below(https://community.nxp.com/docs/DOC-98109) to my BSP,now my booting logo can display from uboot to kernel, there is no any problem. but now the problem is when uboot display the logo, there is a little spash on the screen like below,what's the matter?can you help mekk_image.png

Labels (1)
0 Kudos
Reply
3 Replies

669 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Qiang,

This is due to the resolution of the screen and/or  the size of the picture.

Regards

0 Kudos
Reply

669 Views
1182614726
Contributor III

Hi Bio_TICFSL

the resolution of the screen and the size of the picture both are 1920*1080, and i have change the screen which also supports 1920*1080 resolution, but the display also has the same problem. Maybe i think it's not the primary cause. Can you give me any other suggestions, thank you very much.

0 Kudos
Reply

669 Views
1182614726
Contributor III

Hi Bio_TICFSL

the resolution of the screen supports 1920*1080, and the size of my picture is also 1920*1080. And i have changed another screen which also supports the 1920*1080 resolution.but the picture is also having the same the problem.so maybe you said the issues is not the key of the problem, Do you have any other suggestions, thank you very much.

0 Kudos
Reply