Generator: FAILURE: Error in including

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generator: FAILURE: Error in including

1,054 Views
sarasur
Contributor II

I am a newbie to Freescale Processor Expert.

I am working on i.MX6DL on SABRE Lite board.

I have installed PE in Eclipse environment. I have downloaded components from McuOnEclipse - Browse /PEx Components at SourceForge.net Now after importing these components in PE I am working on the LED Blink project.

I have added LED component from components library. Now when I click Generate Processor Expert Code I get the following error (Check the attached .jpg). Following are my queries

[1] How do I get rid I this error ?

[2] Where is the build file (binary or hex: whichever file is generated for i.MX6DL) saved ?

Any help will be appreciated.

Labels (1)
2 Replies

956 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The following may be helpful :

Integrating Processor Expert for i.MX and ARM GCC with Eclipse


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

956 Views
sarasur
Contributor II

Thank you Yuri,

I built the given sample project at

Integrating Processor Expert for i.MX and ARM GCC with Eclipse using "gcc-arm-none-eabi-4_9-2015q3-20150921-win32 GCC ARM Embedded project files : GCC ARM Embedded " toolchain (however not the Sourcery g++ Lite which you have used as seen in test.map ). Sourcery g++ Lite is now Mentor Graphics product which is available for 30 days evaluation only. So dropped an idea of using it for future developments

However an error "cannot find -lcs3" keeps coming. I am using GNU ARM Eclipse Build Tool for make at GNU ARM Eclipse - Browse /Build Tools at SourceForge.net

May I please know what am I going wrong.

Thanks and regards,

Sarang

integarting_example.jpg

0 Kudos
Reply