I've measured the WAN_EN which should be 1.8v and it reads 3.3v, I cant export the pin as the kernel already has it (I think) so no easy way to change the pin state, but when the pins were used for other functionality at 3.3v they worked without without issue.
WAN_IRQ reads as good as zero.
The pins seem to be setup correctly according to the debug output when the gpio is registered
gpio pin WLAN_EN id 0x3000017 function 3
drive is 1 pull is 0 pullup is 0 output is 1 data is 1
voltage setting exit is 0x0
gpio pin WAN_IRQ id 0x2000019 function 3
drive is 1 pull is 1 pullup is 1 output is 0 data is 0
voltage setting exit is 0x0
the Voltage setting matches PAD_1_8V