Hi,
I am integrating the GainSpan GS2100M module with IMX6SL EVK in Android platform.
Board: IMX6SL EVK
Android version : Kitkat 4.4.2
Kernel Version : Linux 3.0.35
I have driver for the GainSpan GS2100M module. I insert the GainSpan Wifi module in SD1 slot of the IMX6SL EVK board.
I compile the GainSpan driver using .../myandroid/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi- .
It generated the .ko file and i insert the .ko file.
root@evk_6sl:/data/app # insmod gs2k.ko | |
IP2WIFI SDIO Driver Build [Date : Time Stamp] (Apr 20 2015 : 12:25:31) |
gs2k_wlan_sdio: func->num = 0x1 Vendor = 0x296 device = 0x5347 block = 0x800 /
debug_level= 0x0 | |
GS2K mac_address : 20:f8:5e:af:63:04 |
GS2K SDIO Driver Registered 0
After that, I do not know how to integrate the Gain Span module in Android Platform
Any guidance or information to integrate the New WIFI card in Android Platform for IMX6Sl .
Thanks and Regards,
Vinothraj