Suggest to me GSM modules suitable for the imx8mqevk board on the linux platform.
Hello mani0029,
On SabreSDP board, there is a MiniPCIe connector(J1), which is used for connections of 3G/4G module, Slot(con1) is for SIM card, Because 3G/4G module needs the SIM card.
The signal definitions on MiniPCIe is general, you can connect corresponding 3G/4G module with MiniPCIe interface, but you need to port it to android OS by yourself if it is not supported by android BSP we released, before you run SabreSDP board, read corresponding documents firstly, please! you will know what devices or function it supports.
Regards
For the imx8mqevk board, how can I interface the 4G LTE module on linux platform?
Can I use that Quectel module which they mentioned before?
Can I use Quectel UC15, UC21 kit for imx8mqevk for gsm functionality ?
Hi @rmani0029,
You can refer: Quectel UC15, UC21 kit.