GSM modules for imx8mqevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GSM modules for imx8mqevk

1,253 Views
rmani0029
Contributor I

Suggest to me GSM modules suitable for the imx8mqevk board on the linux platform.

0 Kudos
4 Replies

1,236 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello mani0029,

 

On SabreSDP board, there is a MiniPCIe connector(J1), which is used for connections of 3G/4G module, Slot(con1) is for SIM card, Because 3G/4G module needs the SIM card.

The signal definitions on MiniPCIe is general, you can connect corresponding 3G/4G module with MiniPCIe interface, but you need to port it to android OS by yourself if it is not supported by android BSP we released, before you run SabreSDP board, read corresponding documents firstly, please! you will know what devices or function it supports.

 

Regards

 

0 Kudos

1,222 Views
rmani0029
Contributor I

For the imx8mqevk board, how can I interface the 4G LTE module on linux platform?

Can I use that Quectel module which they mentioned before?

0 Kudos

1,226 Views
manizillion
Contributor IV

Can I use Quectel UC15, UC21 kit  for imx8mqevk for gsm functionality ?

0 Kudos

1,248 Views
toanjunifer
Senior Contributor I

Hi @rmani0029,

You can refer: Quectel UC15, UC21 kit.

0 Kudos